Entertainment and special events — such as concerts, festivals, theater performances, sporting events and more — have unique power requirements. These events are often temporary setups that need portable, reliable power sources to work for several hours or days. These power solutions need to support many kinds of equipment, from microphones to speakers to lighting.
Whether your event is small or large, Trystar can provide temporary power for occasions of all kinds. Our products easily and effectively distribute power to support your equipment throughout the event.
Are you holding an event with a bounce house or other similar inflatable amusement devices? We offer Inflatable Party Packages that will easily power your bounce house inflation equipment.
Special Event Power Solutions at Trystar
Trystar has cables, panels, transformers and more for entertainment/event applications. We can customize your productswith your company’s logos and colors so the equipment will fit your branding. We have:
Boxes and Panels
Large-scale events such as concerts will require more than power strips and extension cords to power the stage lighting, sound system and other equipment. Power distribution panels can power all of these components, and you can control individual circuits from the panel.
Our box and panel equipment is available in many sizes and configurations, so you can pick a style that fits your needs. We offer:
Transformers
Some event venues may have a power supply line that doesn’t suit the equipment’s voltage requirements. A transformer will connect the source and equipment to make them compatible, allowing everything to run off a reliable power source.
We have two transformer styles available — dolly style and cage style — that are both portable and durable to get the job done anywhere power is required.
Portable ATS
For entertainment/event performances, the show must go on at all costs, so coordinators need backup plans in case of unreliable power connections or outages. Connecting your audio and visual equipment to a portable generator may be sufficient in some cases, and using a portable automatic transfer switch (ATS) is the best method. The temporary ATS transfers the power from the main source to the generator efficiently so you can maintain your power connection. This method is also safer than extension cords.
Our portable ATS is a durable unit that provides backup power for critical operations. This solution is often used as a temporary fix when the permanent ATS fails.
Entertainment Cable
Entertainment systems require the right cable to establish secure connections. We have many types of cables for events that have worked successfully in large-scale venues. For the entertainment industry, we recommend the stage and lighting cable, which is made for indoor and outdoor use to withstand the elements. It also has internal insulation and a high-contrast cover.
Major Events Trystar Has Powered
Trystar has provided temporary power for events across the United States, so our equipment is tested and proven for reliability in critical applications. We have powered these and many other events:
Request a Quote Today
Since 1992, Trystar has provided event power rentals for sporting events, music festivals, concerts and more. With our power distribution panels, you can count on a reliable power connection for your audio and visual equipment.
Learn more about how Trystar can power your entertainment, sporting or other events by contacting us online. If you know what you need, request a quote today to get temporary power for any occasion.