Trystar - Booth #1475 ARA Show
March 1st – 4th 2026 | Orlando
Powering Possibilities –Designing, engineering, and manufacturing customizable power solutions for industry leaders that demand the best.
Portable Power Solutions
for industry leaders who demand the best.
Powering your mission wherever you need it, Trystar’s portable power solutions are designed to deliver reliability, flexibility, and performance in the most demanding environments. From construction sites to event venues and disaster recovery efforts, our industry-leading equipment ensures safe and seamless power distribution, keeping your operations running smoothly when it matters most. Explore our customizable solutions built to meet the unique needs of your applications.
For Trailer-mounted Load Bank Page: Click Here
For Portable Load Banks Page: Click Here
200A 6P Feeder Panel
The Trystar Power Distribution Panel is built like a tank, from its stainless steel or aluminum enclosure to its heavy duty roll cage. All the components are top of the line. Over the years it has been tested by hard rental and industrial usage, and it has passed with flying colors.
1200A Vertical Power Distribution Panel
Trystar’s UL Listed Power Distribution Panel is equipped with lifting hooks and fork pockets to help you place it into position. These units are built tough and will stand up to heavy rental and industrial use, and can support temporary power needs at events. The Power Distribution Panels feature a hard bus rather than internal cables and offer extra space for additional breakers if you need them.
Step Down/Step Up ISO Transformer Packages
The Trystar Entertainment Transformer is protected by a hefty powder coated cage that can be customized with your company colors. And talk about portability: this unit features lifting points, fork pockets and lockable casters, making it easily transportable for any entertainment application.
200A RV Feeder Panel
The Trystar RV Panel is built like a tank, from its stainless steel or aluminum enclosure to its heavy duty roll cage. All the components are top of the line. Over the years it has been tested by hard rental and industrial usage, and it has passed with flying colors.
Tuff Box
The Trystar Tuff Box is legendary for its rugged simplicity and durability. With OSHA approval, the Trystar Tuff Box has proven itself on countless entertainment and event sites, where it is valued for its lightweight, bulletproof design. Tough enough for the rental and industrial markets, our Tuff Box is one less thing to worry about.
6/4 Cable
These multi-conductor, plug and play cables are very user-friendly and can reduce the number of cables needed on a job site. Trystar Spider Box cables are expertly assembled and factory tested to ensure they work out of the box. Tough enough for the most demanding conditions, they have proven themselves in events and entertainment rental applications.
Quad Box Stringers and Versa-Quads Duplex and GFCI Receptacle
This handy stringer was designed by our engineers to work hard and never come apart. It consists of three rubber outlet boxes which run on three independent circuits. The receptacles within each box are available in GFCI or Edison-style duplex, or a combination of the two.
3 Gang Box
Engineered for reliability, this 3-gang box is built to deliver power where you need it most. Featuring a 20A twist-lock plug and three GFCI duplex receptacles, it’s perfect for safely supplying multiple 120V outlets away from the main panel. Whether you’re powering tools or equipment on a job site or setting up temporary power, this box gets the job done with ease.
10/5 Cable
This handy stringer was designed by our engineers to work hard and never come apart. It consists of three rubber outlet boxes which run on three independent circuits. The receptacles within each box are available in GFCI or Edison-style duplex, or a combination of the two.
EV ChargingPak
The Trystar Portable Electric Vehicle (EV) ChargingPak is an innovative solution designed to provide convenient and reliable charging for electric vehicles on the go, eliminating the need for charging facilities at your event. This compact and versatile charger is specifically developed for the rental market in mind, catering to the growing demand for mobile and portable power solutions. The charger’s compatibility with mobile power solutions ensures that EV owners can access charging facilities even in areas where fixed infrastructure may be limited.
Construction Box
he Trystar Construction Box is legendary for its rugged simplicity and durability. With OSHA approval, the Trystar Construction Box has proven itself on countless entertainment and event sites, where it is valued for its lightweight, bulletproof design. Tough enough for the rental and industrial markets, our Construction Box is one less thing to worry about.
Tuff Panel
Trystar’s UL Listed Power Distribution Panel is equipped with lifting hooks and fork pockets to help you place it into position. These units are built tough and will stand up to heavy rental and industrial use, and can support temporary power needs at events. The Power Distribution Panels feature a hard bus rather than internal cables and offer extra space for additional breakers if you need them.
About Trystar
Trystar LLC designs, engineers, and manufactures customizable electrical power solutions for diverse market sectors, including data centers, utilities, entertainment, education, government, healthcare, and commercial buildings. As an industry leader, Trystar delivers unmatched value and support through its solutions and dedicated team members, ensuring safety, efficiency, and seamless operation for customers who demand the best. Established in 1991, Trystar is headquartered in Faribault, Minnesota, with additional manufacturing facilities and offices across the United States and Canada. Trystar is Powering Possibilities!